私たちのウェブサイトは最高可能なサービスを提供するためにさまざまなクッキーを使用しています。私たちのウェブサイトでのクッキーの使用および注意事項や無効にするための可能性についての情報は私たちの情報ページをご覧ください。あなたの同意により、あなたはクッキーの使用についての情報を読まれたこと、そしてそれに同意されることを確認されることになります。データ保護のテーマについて私たちの詳細情報にも注意してください。

TDK TDK Electronics

About TDK Electronics

[---Image_alt---] Produktspektrum

TDK Electronics (previously EPCOS) develops, manufactures and markets electronic components and systems under the product brands of TDK and EPCOS, focusing on fast-growing leading-edge technology markets, which include automotive electronics, industrial electronics and consumer electronics as well as information and communications technology. Thanks to the 24,000 employees at some 20 design and production locations and an extensive sales network, the company is globally positioned – beyond the provision of standard products – to work closely with customers and create the right solutions for them. 

In fiscal 2018 (ending in March) TDK Electronics posted sales of about EUR 1.6 billion. 

TDK Electronics Headquarters
TDK Electronics AG
Rosenheimer Strasse 141 e
81671 Munich
GERMANY

T +49 89 54020 0
F +49 89 54020 2984
info@tdk-electronics.tdk.com

Products

The diverse range of TDK Electronics portfolio includes capacitors, ferrites and inductors, piezo and protection devices, as well as sensors.

Electronic components and systems are found today in almost every item of electrical equipment, where they are essential for guaranteeing perfect functionality. They perform key functions in cars and trucks, industrial machine tools and in electric railways, wind farms and photovoltaic plants, as well as in washing machines, LED lamps, smartphones, notebooks and televisions. In all these applications TDK Electronics solutions ensure the supply of power, protect electronic circuits and ensure their fault-free operation.

[---Image_alt---] Produktspektrum_CAP

Capacitors are used in all fields of electrotechnology and electronics. They store electric charges and they filter currents and voltages. The portfolio includes aluminum electrolytic, aluminum polymer and film capacitors, whose main applications are in power supplies and converters. Power capacitors ensure a stable supply of power in electric trains, for example. In addition, power capacitors are the key components for the transmission of high-voltage direct current, which enables energy to be transmitted over long distances with minimal loss.
Inductors fulfill two basic functions of electrotechnology, often simultaneously: the filtering of currents and the storage of electromagnetic energy. Ferrites, in turn, constitute the core of inductances and they bundle electromagnetic fields for the transmission of electrical signals and power. Inductors are used, among other things, in switch-mode power supplies for information and communications applications, as well as in automotive, industrial and entertainment electronics. EPCOS also manufactures components that ensure electromagnetic compatibility and, consequently, the fault-free operation of all types of electronic equipment.
[---Image_alt---] Produktspektrum_MAG

[---Image_alt---] Produktspektrum_PPD

Piezo and protection devices protect electronic circuits against voltage spikes and current surges. The portfolio includes surge arresters and switching spark gaps, thermistors, varistors and a comprehensive array of multilayer components that include piezo-actuators, as well as CeraDiode® varistors, the extremely thin CeraPad® substrate with integrated ESD protection, and CeraLink™ capacitors. These components are essential, above all, in vehicles, industrial equipment and household appliances, but also in power engineering, and smartphones, tablets and wearables. Among the latest product highlights are PowerHap™ piezo actuators with haptic feedback, CeraPlas™ for the generation of cold plasma, and CeraCharge™, the world’s first rechargeable solid-state SMD battery.
Sensors and sensor systems include temperature sensors, which, for example, are used in vehicles in systems for reducing emissions. Such components are also used in household appliances and industrial plants. To these must be added the pressure sensors and transmitters that are required primarily for the monitoring and diagnosis of pneumatic and hydraulic systems and for the control of valve and filter systems. One further field of application is medical technology, such as the machines for measuring blood pressure or for artificial respiration. Rounding out the portfolio of sensors is the Tronics product spectrum, which consists primarily of inertial sensors that, among other things, are able to sense acceleration and rotation.
[---Image_alt---] Produktspektrum_TPS


Product Catalogkeyboard_arrow_right